This model is a 2-stage, double-unit type whose stroke length is allowed to exceed the overall length.
General Description (PDF 1,499KB)
| Model
FBL27D | Light load type.
Rail length: 200 to 500mm Stroke: 229 to 524mm | Dimensional Table (153KB) |
| Model
FBL35E-P14 | Light load type.A three-rail, double-slide type that allows a long stroke in a small space. Releasing the automatic free disconnection spring attached on the inner rail allows the inner rail to be pulled out. When folded, the locked state is automatically released with force above a certain level in the folding direction. | Dimensional Table (167KB) |
| Model
FBL35G-P13 | Medium load type. A double-slide type that combines two units of model FBL 35S front-to-front. Releasing the disconnection spring attached on the inner rail allows the inner rail to be pulled out. When folded, the locked state with the disconnect spring is manually released. It is also equipped with a pull-lock mechanism that functions when the slide rail is fully extended. | Dimensional Table (167KB) |
| Model
FBL35G-P14 | Medium load type. A double-slide type that combines two units of model FBL 35S front-to-front. Releasing the automatic free disconnection spring attached on the inner rail allows the inner rail to be pulled out. When folded, the locked state with the disconnect spring can automatically be released with force above a certain level in the folding direction. It is also equipped with a pull-lock mechanism that functions when the slide rail is fully extended. | Dimensional Table (167KB) |
| Model
FBL35D | Medium load type. A double-slide type that combines two units of model FBL 35S back-to-back. It is extensively used regardless of the industry. | Dimensional Table (165KB) |
| Model
FBL35W | Medium load type. A double-slide type based on model FBL 35S that achieves a thickness of one single-slide unit. | Dimensional Table (174KB) |
| Model
FBL51H | Medium load type. A three-rail, double-slide type that allows a long stroke. With the smallest thickness, this model can be used in a space-saving location even under a large load. | Dimensional Table (163KB) |
| Model
FBL51H-P13形 | Medium load type. A three-rail, double-slide type that allows a long stroke. With the smallest thickness, this model can be used in a space-saving location even under a large load. Releasing the disconnection spring attached on the inner rail allows the inner rail to be pulled out. When folded, the locked state with the disconnect spring is manually released. It is also equipped with a lock mechanism that functions when the slide rail is fully extended. | Dimensional Table (171KB) |
| Model
FBL51H-P14 | Medium load type. A three-rail, double-slide type that allows a long stroke. With the smallest thickness, this model can be used in a space-saving location even under a large load. Releasing the automatic free disconnection spring attached on the inner rail allows the inner rail to be pulled out. When folded, the locked state is automatically released with force above a certain level in the folding direction. | Dimensional Table (172KB) |
| Model
FBL35K | Heavy load type. A double-slide type combining 4 units of model BFL 35S. It achieves the largest permissible load among all types and is optimal for opening/closing heavy objects. | Dimensional Table (169KB) |
| Model
FBL56H | Heavy load type.
Rail length: 305 to 762mm Stroke: 330 to 787mm | Dimensional Table (159KB) |
| Model
FBL56H-P13 | Heavy load type. A double-slide type with the largest permissible load among the three rails. Releasing the disconnection spring attached on the inner rail allows the inner rail to be pulled out. When folded, the locked state with the disconnect spring is manually released. It is also equipped with a lock mechanism that functions when the slide rail is fully extended. | Dimensional Table (175KB) |
| Model
FBL56H-P14 | Heavy load type. A double-slide type with the largest permissible load among the three rails. Releasing the automatic free disconnection spring attached on the inner rail allows the inner rail to be pulled out. When folded, the locked state is automatically released with force above a certain level in the folding direction. | Dimensional Table (167KB) |