THK
Global Top

HOME > THK Technology > Product Information

 
Product Information

Let's introduce our product lines. Summarized below are broad categories of THK products. For further information about the products, refer to our technical support site.

Retainer-embedded roller guides
Retainer-embedded roller guides
Ultra super rigid, difficult load, low friction
Global standard dimensions (installation compatible)
Ball-retainer-embedded LM guides
Ball-retainer-embedded LM guides
Ensures long life and long-term maintenance free operation.
The retainer-embedded roller guides adopt a roller retainer to prevent the introduction of skew, realizing low-friction smooth motions. They are ultra super rigid roller guides that offer long maintenance-free operation.

The ball-retainer-embedded LM guides are retained by ball retainers and circled so that they are free from mutual friction between the balls. In addition, a grease pocket is formed between the balls and retainer. This increases the grease's retention capability, ensuring long maintenance free operation.

LM guides
LM guides
Rolling linear guides available in a wide variety of types
Ball splines
Ball spline
Realize torque-transferable direct-acting rolling motions.
The THK's LM guides form epoch-making motion systems that make linear motions into rolling motions. They apply the rotation theory of the "well base ball bearing," which is the easiest to use and most economical rolling bearing, to the linear motion parts. The type of contact between the rolling surface and the ball has been transformed from "rolling contact" toward "surface contact" by providing R-shaped grooves with a radius close to that of the balls on the rolling surface.

A ball spline is an epoch-making direct motion system in which the balls embedded in the spline external cylinder can convey torque while making a linear motion smoothly in the rolling groove of the precisely ground spline shaft.

High-precision ball screws
High-precision ball screws
Can offer a highly precise rolling feed mechanism.
Rolling ball screws
Rolling ball screws
Provide low-cost rolling lead screws.
A wide variety of high-precision ball screws are available as standard parts so that the users can select the most suitable part according to their application. Also available as a series are a line of nut-screwing ball screws which are suitable not only for conventional shaft rotation use but also for nut screwing.

THK's rolling ball screws are low-cost lead screws which adopt a screw shaft that is subjected to thread rolling and special surface grinding finishing instead of an expensive screw ground shaft.

Linear bushings
Linear bushings
Inexpensive yet highly precise direct motion systems
Cross roller rings
Cross roller rings
A single bearing can carry loads that are put in all directions.
THK's linear bushings are direct motion systems that, used in combination with a hardened shaft, give infinite linear motions. Since their load balls and hardened shaft make point contacts, they set up linear motions at a minimum frictional resistance and offer highly precise smooth motions though their permissible load is rather low.

Since cross roller rings are arranged so that they alternate orthogonally with each other on a 90-degree V-groove-shaped rolling surface through spacer retainers; a single bearing can carry loads that are put in all directions, including radial, axial, and moment loads.

Rotary series
Rotary series
Available are a series of cam and roller followers.
Spherical joints
Spherical joints
Spherical bearing/rot-end ring ball series
THK's cam and roller followers are compact and rigid bearings which, incorporate needle bearings, and are used as cam mechanisms and linear motion guide rollers, respectively.

THK's spherical bearings are self-aligning slide bearings for carrying heavy loads. The rot end provides play-free and extremely smooth rotational and oscillating motions. The ring balls excel in wear resistance and realize clearance-free smooth motions.
Actuators
Actuators
Actuators that make use of the LM guide technology
Units
Units
An orchestration of THK technologies
These are a series of actuators that combine guides, ball screws, and linear motors. THK offers a line of actuators in wide variations including one-shaft type and those which permits 2 or 3 shafts to be combined.

Units refer to tables that combine the LM guide and ball screws in an XY configuration and offer high-precision feeds. They are the results of combining THK's best technologies and include standard tables, hollow tables, and tables that automatically correct misalignments.


To Top of this page
To Top of THK Technology


Site MapPrivacyLegalExport SecurityContact Us