THK
Global Top

HOME > THK Technology > Supporting Society

Society
Supporting Society

Making contributions for the foundation of social infrastructures and better industrial development.

By observing the foundation of modern society, we can see that it is buttressed with various technologies. For instance, in the infrastructure of modern society new technologies are continuously developed in order to accommodate an unsettled and ever-changing society, and these technologies fertilize society so new businesses and life-styles can emerge and grow. THK's unique technologies support the bases of society such as information technology (IT), transportation systems, civil engineering and architectural work, or even food life and urban function design to help create new values in our lives. This is one of THK's tasks.

Shield Machine
Illustration above: Shield Machine
Let's take a closer look. Communication infrastructure that will change the world is also an important issue for the future of Japan. In this field, an optical fiber network is considered the nerve system of modern society. Even though the construction of the infrastructure has also been embarked upon in Japan, improvements for greater reliability is an important issue for the "nerve system." This is where our "optical fiber inspection machine" comes in. This inspection machine is compactly built with "LM Guides," "Ball Screws" and "Challenges" and has very precise positioning capability. By grasping each stem of the nerve system, a dramatic reliability improvement can be achieved, and such precise inspection supports providing a safe and comfortable next generation network.

It is most likely that the optical fiber network will be facilitated underground. This underground position has great possibilities and importance, not only for communication, but also for transportation purposes. Particularly, in urban areas where the surface level is already saturated, it is mandatory to facilitate an underground transportation infrastructure. In this field, "Shield Machines (excavation machines)" are utilized for excavating underground tunnels. For instance, a larger scale shield machine for excavating tunnels for metropolitan railway systems is equipped with THK's "Big Scale LM Guide" in its robot parts which remove concrete pieces to the surface and implement precise installation.

It may be surprising to see that such large scale civil engineering facilitation is supported by technological elements that are small enough to hold in your hands. For joint parts and the control levers of construction equipment used in construction and civil engineering work, THK's "Spherical Axis Modules", "Ring Balls" and "Rod Ends" are utilized.
We would like you to see these THK's parts in our showroom in person. You can experience firsthand the reality that big projects are supported by small but powerful technologies.

"R Guide" is a good example of a technology or product that possesses power and smoothness. This technology is utilized in pendulum vehicles such as the limited express trains used by Japan Railways and was developed to improve the speed of those trains that run on conventional lines. In areas where rail lines curve, the speed of a train can be increased by tilting the wheels toward the inside similar to a motorcycle. "R Guide" realizes this mechanism by forcibly and smoothly tilting and supporting the wheels. "R Guide" is used on the "Super Aozora" train which operates between Sapporo and Kushiro and the "Shinano" train which operates between Nagoya and Nagano. This technology brings about not just speed improvement between these cities but also immeasurable economic benefits. THK's outstanding technology can provide such side effects.

THK's technologies also make appearances in many other places such as mechanized parking building systems which support the urban economy and rice-transplanting vehicles which increase agricultural productivity. Palm size pieces of machinery support and buttress large societies. Using innovative ideas and the power of creative thinking,THK continues to manipulate and develop new technology.


For more details on each of our products, please refer to Product Information

To Top of this page
To Top of THK Technology
To the Future---Changing the Way We CreateLife---Protecting Life Daily Life---Enriching LifeMother Earth---Walking with Mother Earth

Site MapPrivacyLegalExport SecurityContact Us