THK Global


Home > “OMNIedge” IoT Service for the Manufacturing Industry at Hannover Messe

"OMNIedge" IoT Service for the Manufacturing Industry
at Hannover Messe

March 29, 2019

THK CO., LTD. will be exhibiting at HANNOVER MESSE, held April 1–5, 2019, in Hannover, Germany. THK’s booth will feature its mainstay LM Guides, ball screws, and electric actuators. In addition, a special area of the booth will be reserved for the trade show debut of OMNIedge, a simple, secure, and global predictive failure detection application for the manufacturing industry. A demonstration of this new service will be provided. As the service is scheduled to launch in the European market in during 2020, THK will begin seeking customers to participate in a free trial this year.

OMNI edge IoT Service for the Manufacturing Industry

Hannover Messe

Exhibition

Hannover Messe

Venue

Hannover Exhibition Grounds, Hannover, Germany

Date

April 1 - 5, 2019
9:00 - 18:00

Booth

Hall 17, C42

Registration

VISITOR PRE-REGISTRATION FORM

Challenges Facing the Manufacturing Industry

With regard to the manufacturing industry in developed countries, the aging of society and other factors have led to turnover, raising concerns about worsening labor shortages. As a result, there is a greater need for automating regular inspections of equipment, which currently rely on manual labor, and creating a system for predictive failure detection. Manufacturers of production equipment are independently attempting to collect data from control devices and visualize the condition of their equipment.
However, even when they can detect overall issues with the machine, those manufacturers must rely on the instincts of experienced maintenance personnel to identify which component has failed. In addition, even when a company can obtain data from each component, they are often unable to predict failures because they cannot analyze the data without possessing specialized knowledge about those components.
Furthermore, companies are often unable to install an IoT system that visualizes machine conditions because of the specialized IT knowledge required to connect the system to the factory’s network, as well as the high initial and operating costs.

 

The THK SENSING SYSTEM

To solve the issues facing manufacturing, THK developed the “THK SENSING SYSTEM.” Through the use of sensors, which can be installed on current equipment, this technology collects and visualizes information about the condition of LM Guides* and ball screws, which are critical machine components.
Because this technology directly measures and analyzes the condition of a critical component that can lead to malfunctions, rather than the entire machine, it makes it possible to identify the damaged part.

THK SENSINT SYSTEM

THK’s New IoT Service for the Manufacturing Industry: OMNIedge

Predictive failure detection will be made possible using THK’s new OMNIedge service to take data collected by the THK SENSING SYSTEM and a Cisco edge computing router or a smartphone and gather it securely through DOCOMO’s mobile network. THK can provide an application that will enable the diagnosis of an LM Guide’s or ball screw’s condition and the predictive maintenance of equipment by using data collected through the THK SENSING SYSTEM.
The greatest feature of OMNIedge is that it automates the design and setup work necessary for introducing the IoT, including data collection, storage, and analysis. As a result, this system can be quickly and easily installed even in manufacturing facilities without IT staff. Total support is also available for maintenance and operation, which reduces the burden on customers.
*LM Guides, or linear motion guides, enable the linear motion of machines through rolling motion.
THK is the manufacturer with the leading market share worldwide in linear motion guides (according to a 2017 THK study).

 

OMNI edge

Contact

THK CO., LTD.  IOT Innovation Division
OMNIedge Section
Contact form