1. Home
  2. Product Information
  3. Product News
  4. THK Resumes Production of Oil-Free LM Guide Model SR-MS for Special Environments

THK Resumes Production of Oil-Free LM Guide Model SR-MS for Special Environments

THK CO., LTD. (Location: Minato, Tokyo; President: Takashi Teramachi; hereinafter referred to as “THK”) has resumed production of the Oil-Free LM Guide Model SR-MS for Special Environments.

Oil-Free LM Guide Model SR-MS for Special Environments
Oil-Free LM Guide Model SR-MS for Special Environments

The Model SR-MS is an LM Guide that utilizes a highly reliable dry lubrication S-compound film to provide its stainless steel balls with grease-free lubrication. Its low-outgassing properties make it suited to a variety of environments, from regular atmospheric pressure to vacuums. All of the components are made of stainless steel, so it can also be used in temperatures up to 150°C (or at an instantaneous temperature of 200°C).

Production of this product has been on hold since July 2022, but in response to increased interest expressed by our customers, we have now resumed production.

THK will continue striving to provide our customers with a stable supply of diverse products and propose offerings that meet their requirements. We appreciate your continued support.

Related information

Learn more about the Oil-Free LM Guide Model SR-MS for Special Environments here

Contact information

For more detailed information, please contact THK directly:

THK GmbH
PR Group
+49 2102 7425-151
press@thk.eu
www.thk.com