Copy item link
Add item to favorites
Do you offer a preloaded product for the Rolled Ball Screw?
Yes. Model JPF is the preloaded type of the Rolled Ball Screw.

The direction of the applied load to the Model JPF during use must be the same as the recommended loading direction illustrated in the figure. If a load is applied from the opposite direction, it results in the decrease of the preload and damage to the spring structure. To avoid this, make sure that the applied load remains 0.1 x Ca or below during use.