Europe
To FAQ
Copy item link
Add item to favorites
How much grease should be injected into the LM Guide?
The amount is approximately 30% to 60% of the block's internal volume.
The actual amount varies depending on the model number.