Copy item link
Add item to favorites
What precautions should I take when removing an LM block from an LM rail?
The balls may fall out if an LM block is removed from an LM rail.
Do not remove an LM block from an LM rail during setup. If removing the LM block is inevitable due to the plate cover type or the assembly procedure, be sure to use the removing/mounting jig.
Note that the removing/mounting jig is not included in the LM Guide package as standard. To obtain one, contact THK.

For the removing/mounting jig, click here.

For inquiries, click here.