Can model HSR guide clamper CP-H also be used on other models?
Yes, it can be used on other models, too, depending on model and size. However, dimensions must be checked since its shape differs from model HSR. For example, in the case of model SHS, the rail height on models HSR and SHS is different. So, a clearance is formed between the guide clamper and the table when model SHS is chosen. Inserting spacers for adjusting the clearance enables model SHS to be used. There are also other types, such as models SR and SSR, that can be used. Contact THK about whether or not they can be used and spacer dimensions.