Copy item link
Add item to favorites
What are the mounting surface tolerances for the Curved LM Guide Model HCR (error allowance in parallelism between two rails and error allowance in vertical level between two rails)?
They are the same as the tolerances for the Model HSR.
For the curved LM Guide, the error allowance in parallelism between two rails is a value relative to a reference radius R.
Mount the reference side LM rail to the reference R carefully, using an abutting surface or similar tool.

    For accuracy standards, click here.

    For the mounting procedure, click here.