Europe
To FAQ
Copy item link
Add item to favorites
What is the temperature factor if the working temperature exceeds 200°C?
Since 200°C is out of the working temperature range, the temperature factor at 200°C has not been set. You can use the LM Guide for high temperatures up to 150°C.