Copy item link
Add item to favorites
Is it possible to prevent the cage of a cross-roller guide or ball guide from becoming misaligned?
The roller cage of a conventional Model VR or Model VB may drift when affected by factors such as a moment, vertical mounting, or machine vibrations.
If cage drift will be a problem, we recommend using the Model VRG cross-roller guide, which has a mechanism to prevent misalignment of the cage, or an LM Guide system that circulates rolling elements endlessly.