Copy item link
Add item to favorites
What do we have to bear in mind when installing the Cam Follower in a place where it applies heavy loads?
It needs to be installed so that the stud oil holes are not located to the load area. The oil holes are located on the side of the stud flange marked with a THK logo.