1. Home
  2. Product Information
  3. LM Guide
  4. Precautions on Use

LM Guide Precautions on Use

Precautions on Using the LM Guide

Handling

  1. Please use at least two people to move any product weighing 20 kg or more, or use a dolly or another conveyance. Doing so may cause injury or damage.
  2. Do not disassemble the parts. This will result in loss of functionality.
  3. Tilting an LM block or LM rail may cause them to fall by their own weight.
  4. Take care not to drop or strike the LM Guide. Doing so may cause injury or damage. Giving an impact to it could also cause damage to its function even if the product looks intact.
  5. Do not remove the LM block from the LM rail during setup.
  6. Do not insert hands or fingers into the mounting holes on the LM rail, as they could get caught between the rail and the LM block, resulting in injury.
  7. To ensure personal safety, wear gloves and protective footwear when handling this product.

Precautions on Use

  1. Prevent foreign material, such as cutting chips or coolant, from entering the product. Failure to do so may cause damage.
  2. If the product is used in an environment where cutting chips, coolant, corrosive solvents, water, etc., may enter the product, use bellows, covers, etc., to prevent them from entering the product.
  3. Do not use this product if the external temperature exceeds 80°C. Unless the unit is specially designed to be heat-resistant, exposure to such temperatures may deform or damage plastic and rubber parts.
  4. If foreign material such as cutting chips adheres to the product, replenish the lubricant after cleaning the product.
  5. Micro-strokes tend to obstruct oil film to form on the raceway in contact with the rolling element, and may lead to fretting corrosion. Take consideration using grease offering excellent fretting prevention. It is also recommended that a stroke movement corresponding to the length of the LM block be made on a regular basis to make sure oil film is formed between the raceway and rolling element.
  6. Do not use undue force when fitting parts (pin, key, etc.) to the product. This may generate permanent deformation on the raceway, leading to loss of functionality.
  7. If, for operational reasons, it becomes absolutely necessary to remove the LM block from the LM rail and reattach it, a special mounting jig must be used for this purpose. (The mounting jig is not included with standard versions of the product. To obtain one, please contact THK.)
  8. Position the mounting jig so that one end abuts the end of the LM rail. When the rail and the jig are exactly aligned, the LM block can be loaded onto the rail.
  9. Take care to keep the LM block straight. Loading the block at an angle can introduce foreign matter, damage internal components, or cause balls to fall out.
  10. The LM block must contain all its internal rolling elements (balls) when mounted on the LM rail.Using a block with any balls removed may result in premature damage.
  11. Please contact THK if any balls fall out of the LM block; do not use the block if any balls are missing.
  12. If the LM Guide breaks due to an accident or other cause, the block may come off of the rail and fall. For the safe use of this product, take precautions such as adding a mechanism to prevent the block from falling.
  13. For bolt length, select a length that will leave a clearance at the bolt tip in relation to the effective tap depth.
  14. Insufficient rigidity or accuracy of mounting members causes the bearing load to concentrate on one point and the bearing performance will drop significantly. Accordingly, give sufficient consideration to the rigidity/accuracy of the housing and base and strength of the fixing bolts.
  15. When removing the LM block from the LM rail and then replacing the block, an LM block mounting/removing jig that facilitates such installation is available. Contact THK for details.

Lubrication

  1. Thoroughly remove anti-rust oil and feed lubricant before using the product.
  2. Do not mix different lubricants. Mixing greases using the same type of thickening agent may still cause adverse interaction between the two greases if they use different additives, etc.
  3. When using the product in locations exposed to constant vibrations or in special environments such as clean rooms, vacuum and low/high temperature, use the grease appropriate for the specification/ environment.
  4. When lubricating the product having no grease nipple or oil hole, apply grease directly on the raceway and stroke the product several times to let the grease spread inside.
  5. The consistency of grease changes according to the temperature. Take note that the slide resistance of the LM Guide also changes as the consistency of grease changes.
  6. After lubrication, the slide resistance of the LM Guide may increase due to the agitation resistance of grease. Be sure to perform a break-in to let the grease spread fully, before operating the machine.
  7. Excess grease may scatter immediately after lubrication, so wipe off scattered grease as necessary.
  8. The properties of grease deteriorate and its lubrication performance drops over time, so grease must be checked and added properly according to the use frequency of the machine.
  9. Although the lubrication interval may vary according to use conditions and the service environment, lubrication should be performed approximately every 100 km in travel distance (three to six months).<br/>Set the final lubrication interval/amount based on the actual machine.
  10. If the mounting orientation is other than horizontal use, the lubricant may not reach the raceway completely. For the mounting orientation and the lubrication, see Setting Conditions and Lubrication, respectively.
  11. When adopting oil lubrication, the lubricant may not be distributed throughout the LM block depending on the mounting orientation of the block. Contact THK in advance for details.

Storage

When storing the LM Guide, enclose it in a package designated by THK and store it in a room in a horizontal orientation while avoiding high temperature, low temperature and high humidity.
After the product has been in storage for an extended period of time, lubricant inside may have deteriorated, so add new lubricant before use.
If you request that we do not apply anti-rust oil to a product, please be aware that it may rust due to the storage environment or length of storage.

Disposal

Dispose of the product properly as industrial waste.

Precautions on Handling the LM Guide for Special Environment

LM Guide for Medium-to-Low Vacuum

Handling

  1. This product has been thoroughly cleaned and degreased and then sealed in moisture-proof packaging. If possible, open the package immediately prior to using the product.
  2. Once the packaging has been opened, store the product inside a clean, dry receptacle accompanied by silica gel or another drying agent. Do not use anti-rust oil or corrosion- or tarnishpreventive paper or fluid with this product.
  3. Wear protective rubber or vinyl gloves while handling this product and make sure the surrounding environment is relatively clean.

Precautions on Using Options for the LM Guide

QZ Lubricator for the LM Guide

QZ Lubricator

Precaution on Selection

Secure a stroke longer than the overall LM block with QZ Lubricator attached.

Handling

Take care not to drop or strike this product. This could cause injury or product damage.Do not block the vent hole with grease or the like.
The QZ device supplies oil only to the raceway, so use it in combination with regular greasing/lubrication. If the product is used in an environment exposed to coolant, cutting chips or other foreign material, oil on the raceway is lost easily. Accordingly, be sure to also use covers, bellows, etc.

Service environment

Be sure the service temperature of this product is between ‒10 to 50°C, and do not clean the product by immersing it in an organic solvent or white kerosene, or leave it unpacked.

Precautions on Using Options for the LM Guide

LaCS
Side Scraper

Handling

The lubricant impregnated into the scraper is used to increase its sliding capability. For lubrication of the LM Guide, attach QZ Lubricator, or the grease nipple on the side face of the end plate of the LM block, before providing a lubricant.
When using the product, be sure to attach the rail cap C or the plate cover.

Service environment

Be sure the service temperature of this product is between -20 to +80°C, and do not clean the product by immersing it in an organic solvent or white kerosene, or leave it unpacked.

Notes on the Product Functions

It is specifically designed to provide dust prevention capability to remove foreign material and liquid.To seal oil, an end seal is required.

Light Contact Seal LiCS for LM Guides

LiCS

Handling

The lubricant impregnated into LiCS is used to increase its sliding capability. For lubrication of the LM Guide, attach the grease nipple on the end plate of the LM block before providing a lubricant.

Service environment

Be sure the service temperature of this product is between -20 to +80°C, and do not clean the product by immersing it in an organic solvent or white kerosene, or leave it unpacked.
It contacts only with the LM rail raceway. Do not use it in harsh environments.

High Chemical Resistance Fluorine Seal FS for the LM Guide

Fluorine Seal FS

Handling

Be careful not to twist the seal portion when attaching the fluorine seal to the LM Guide. Also, do not store the product in a way that may deform the seal, such as by stacking it. This may cause damage or reduce the seal’s functionality.

Service environment

The service temperature range is between -20°C and 80°C. Avoid cleaning with organic solvents or kerosene, and do not store unwrapped for extended periods of time.

Cap GC

Cap GC

Handling

If GC caps are specified for the product, the edges of the LM rail mounting hole openings will be sharp. Take great care not to injure your fingers or hands while working.
When fitting GC caps, use a flataligning tool to gradually punch the cap into the hole until it is level with the upper surface of the LM rail. Then run an oil stone over the rail until the upper surface of the rail and the GC caps are completely flat.
When installing or removing, burrs and small debris on the cap may scatter, so be sure to wear protective goggles and avoid using sharp tools during work.