Guide Ball Bushing Precautions on Use
Handling
- Disassembling each part may cause dust to enter the system or degrade mounting accuracy of parts. Do not disassemble the product.
- Take care not to drop or strike the Linear Bushing. Doing so may cause injury or damage. Giving an impact to it could also cause damage to its function even if the product looks intact.
- When handling the product, wear protective gloves, safety shoes, etc., as necessary to ensure safety.
Precautions on Use
- Prevent foreign material, such as cutting chips or coolant, from entering the product. Failure to do so may cause damage.
- If the product is used in an environment where cutting chips, coolant, corrosive solvents, water, etc., may enter the product, use bellows, covers, etc., to prevent them from entering the product.
- Do not use the product at temperature of 80℃ or higher. Exposure to higher temperatures may cause the resin/rubber parts to deform/be damaged.
- If foreign material such as cutting chips adheres to the product, replenish the lubricant after cleaning the product.
- Micro-strokes tend to obstruct oil film to form on the raceway in contact with the rolling element, and may lead to fretting corrosion. Take consideration using grease offering excellent fretting prevention. It is also recommended that a stroke movement corresponding to the length of the outer cylinder be made on a regular basis to make sure oil film is formed between the raceway and rolling element.
- Do not use undue force when fitting parts (pin, key, etc.) to the product. This may generate permanent deformation on the raceway, leading to loss of functionality.
- Insert the shaft straight through the opening. Inserting the shaft at an angle can introduce foreign matter, damage internal components, or cause balls to fall out.
- Using this product with any balls removed may result in premature damage.
- Please contact THK if any balls fall out; do not use the product if any balls are missing.
- If an attached component is insufficiently rigid or mounted incorrectly, the bearing load will be concentrated at one location and performance will decline significantly. Make sure the housing and base are sufficiently rigid, the anchoring bolts are strong enough, and the component is mounted correctly.
Lubrication
- Thoroughly wipe off anti-rust oil and feed lubricant before using the product.
- Do not mix different lubricants. Mixing greases using the same type of thickening agent may still cause adverse interaction between the two greases if they use different additives, etc.
- When using the product in locations exposed to constant vibrations or in special environments such as clean rooms, vacuum and low/high temperature, use the grease appropriate for the specification/environment.
- To lubricate the product, apply lubricant directly to the raceway surface and execute a few preliminary strokes to ensure that the interior is fully lubricated.
- The consistency of grease changes according to the temperature. Take note that the slide resistance of the Linear Bushing also changes as the consistency of grease changes.
- After lubrication, the slide resistance of the Linear Bushing may increase due to the agitation resistance of grease. Be sure to perform a break-in to let the grease spread fully, before operating the machine.
- Excess grease may scatter immediately after lubrication, so wipe off scattered grease as necessary.
- The properties of grease deteriorate and its lubrication performance drops over time, so grease must be checked and added properly according to the use frequency of the machine.
- The greasing interval varies depending on the use condition and service environment. Set the final lubrication interval/amount based on the actual machine.
Assembling the LG Nut with the LG Shaft of the Guide Ball Bushing
- When assembling the LG nut with the LG shaft, align the position of the balls inside the LG nut with the position of the groove of the LG shaft, then insert the LG shaft into the LG nut straightforward and gradually. If the LG shaft is tilted when it is inserted, balls may bounce out or damage the circulating part.
- If the LG shaft is stuck in the middle of insertion, do not force it into the nut. Instead, but pull it out first, re-check the ball position and the LG shaft groove position, and then insert it straightforward and gradually.
- After assembling the LG nut with the LG shaft, check that the LG nut or the LG shaft smoothly moves. If the shaft was forced into the nut, function could be lost even if the product looks intact.
Storage
When storing the Guide Ball Bushing, enclose it in a package designated by THK and store it in a room while avoiding high temperature, low temperature and high humidity.
If you request that we do not apply anti-rust oil to a product, please be aware that it may rust due to the storage environment or length of storage.
Disposal
Dispose of the product properly as industrial waste.