Copy item link
Add item to favorites
Is there any way of learning (inspection method) the state of deterioration of LM guides on equipment that has been used for a long time?
Check the following as LM guide inspection items:
- Abnormalities (flaking or scratching) in raceway?
- Lubricant adhering to raceway?
- Metal fragments near raceway (flakes, etc. on raceway surface)?
If an abnormality occurs
- Accuracy (positional accuracy, running accuracy) becomes out of order
- Quality of machined surfaces drops (machine tool, etc.)
- Abnormal sound, vibration, etc. occurs. Check the above items during inspection.