1. Home
  2. Product Information
  3. Product News
  4. Utility Slide Model ATG Product Lineup Expanded with New Model ATG43

Utility Slide Model ATG Product Lineup Expanded with New Model ATG43

THK CO., LTD. (Location: Minato, Tokyo; President: Takashi Teramachi; hereinafter referred to as “THK”) has expanded the lineup of its Utility Slide Model ATG with the new Model ATG43.

Utility Slide Model ATG
Utility Slide Model ATG

The Model ATG is a finite type linear motion guide device composed of a U-shaped outer member with two grooves and an inner member on the inside. It combines the special features of conventional slide rails with the technology THK has cultivated with the LM Guide to provide a greater permissible load and longer service life to meet the needs of the logistics and railway industries. In addition, this product possesses two rows of balls that provide smooth, stable movement, and it can also be mounted with an ease unique to slide rails.

THK has now added the new Model ATG43 to its existing lineup that includes Models ATG22, 28, and 35. It will satisfy the needs of the logistics and railway industries in places like automated distribution warehouses, the opening/closing mechanisms of railway doors, and the sliding mechanisms of airplane passenger seating.

THK will continue to use the technology and know-how it has cultivated as a top manufacturer of machine components to develop and provide products that meet the needs of customers in a variety of fields.

Related information

Product Information for Utility Slide ATG

Note) This information was originally released in Japanese on September 11, 2024.

Contact information

Please direct any media inquiries to:

Toru Nakagawa & Akio Ishikawa, Marketing & Public Relations Department, THK CO., LTD.
Phone: +81-3-5730-3845
E-mail: thk-sp@thk.co.jp