1. Home
  2. Product Information
  3. Product News
  4. THK Original PFAS-Free Vacuum Grease Now Available, Providing Cleanliness and Smooth Motion Even in Vacuum Environments

THK Original PFAS-Free Vacuum Grease Now Available, Providing Cleanliness and Smooth Motion Even in Vacuum Environments

THK CO., LTD. (Location: Minato, Tokyo; President: Takashi Teramachi; hereinafter referred to as “THK”) is now accepting orders for THK Original PFAS-Free Vacuum Grease (Model: AFPF).

PFAS-Free Vacuum Grease (Model: AFPF)
PFAS-Free Vacuum Grease (Model: AFPF)

In recent years, Europe, the Americas, and other parts of the world have been strengthening regulations around the use of PFAS (organofluorine chemical compounds), which are believed to have a negative effect on human health. While fluorinated grease is often used in vacuums and other special environments, the PFPE (perfluoropolyether) and PTFE (polytetrafluoroethylene) that it is made of are exposed to increased risk of future restrictions being placed on their use, manufacture, and importation.

In light of the possibility of such environmental restrictions, we have developed THK Original PFAS-Free Vacuum Grease.

Manufactured using PFAS-free and metal-free formulas and processes, this grease is optimized for linear motion products, and it provides the kind of low steam pressure, low sliding resistance, low dust generation, and low outgassing performance that is indispensable to vacuum applications. It reduces the risk of contamination inside of semiconductor manufacturing equipment, and it offers both smooth motion and superior lubrication performance.

THK will continue to use the technology and know-how it has cultivated as a top manufacturer of machine components to develop and provide products suited to various environments so as to meet the needs of customers.

Features

Usable in high vacuum environments
This grease offers low steam pressure and low outgassing performance, which make it usable in high vacuum environments.

Low sliding resistance
With its low sliding resistance, this grease excels at rolling stability.

Low dust generation
Thanks to its extremely low level of dust generation, this grease can be used without contaminating the surrounding environment.

* Here, "PFAS-free" and "metal-free" mean that there is no intentional inclusion of fluorine, fluorine compounds, or metallic elements such as copper, zinc, or lithium in the composition of this grease or in its manufacturing processes.

* Please notify THK in advance if you are considering selling or using this product in a country or region outside of Japan.

Related information

Learn more about THK Original PFAS-Free Vacuum Grease here

Note:This information was originally released in Japanese on April 30, 2026.

Contact information

Please direct any media inquiries to:

Marketing & Public Relations Department, THK CO., LTD.
Phone: +81-3-5730-3845
E-mail: thk-sp@thk.co.jp