Copy item link
Add item to favorites
I can operate the TSC/TLC/THC driver controllers using the PC setup tool D-STEP or the digital operator TDO-N, but I can't operate them using the I/O. What should I do?
To issue commands from the I/O, you must set the function mode to AUTO.
Please check that the mode switch on the front of the controller is not set to MANU.

Also, if the mode switch is in AUTO mode and it still does not work, it may be paused.
Wire the I/O pause input (b contact), or disable the pause input selection in the parameters.