Copy item link
Add item to favorites
Can the home position of the CLM be changed?
The home position cannot be changed after purchasing the CLM.
Locations where the CLM home position can be set are spaced at 50 mm intervals.
The position to be used as the home is set by installing an S-pole magnet.
If you specify the home position prior to purchase, we will install the S-pole magnet in the position closest to the location you select.