- The load capacity listed for PC/PCT is for vertical use, but can these models be used horizontally?
And if so, what is the load capacity when doing so?
- Yes, they can be used horizontally.
Prepare a separate guide mechanism if a radial load or moment will be applied to the rod.
Contact THK for details.
For inquiries, click here.