To FAQ
Copy item link
Add item to favorites
For a Model SKR with two blocks (B/D type), how should the distance between the blocks be specified?
When there are two blocks, one of them will not be machined for use as a ball screw nut.
The distance between the blocks can be adjusted freely.