What problems may occur if I add a grease that is different from the type used for initial lubrication?
If a different grease is used than the pre-packed grease, the lubrication performance may be reduced, or the properties of the grease may change depending on the compatibility of the two greases.
Generally, if the greases use the same thickening agent, they are unlikely to cause major problems, but caution is required as there is a possibility that a problem will occur.
When using a different grease, wipe off as much of the initial AFB-LF grease as possible, then add the new grease to be used.
Flush the remaining grease from inside the inner block by repeatedly injecting the new grease.