- Can the service life of the Curved LM Guide Model HCR be calculated?
- The service life of the Curved LM Guide Model HCR can be calculated.
When selecting a model, however, keep in mind that the orientation in which the Curved LM Guide Model HCR is used will change the direction of the load acting on the block.
Contact THK for details.
For inquiries, click here.