For products without a grease nipple, how should I replenish grease?
If there is no grease nipple, please replenish grease using the following methods.
1. If there is a lubrication hole:
Replenish grease using a commercially available syringe, inserting the nozzle of the syringe into the lubrication hole.
The lubrication hole diameter varies depending on the model number, so please refer to the general catalog for details.
2. If there is no grease nipple or lubrication hole:
Apply grease directly to the groove of the LM rail and perform a warm-up operation to allow the grease to break in sufficiently.