Copy item link
Add item to favorites
What is the positioning accuracy of the LM Guide?
The LM Guide is good at subtle motion because it moves more lightly than the slide guide. The LM guide can make an accurate stop at a designated position under numerical control. It also follows feed in nanometers, but this depends on the precision of the driving unit. Note that pitching and yawing will affect the positioning accuracy.