Copy item link
Add item to favorites
Are there any maintenance-free LM Guides?
Only the amount of grease sealed in the LM Guide with caged balls at the factory is sufficient for use in a normal environment. Even if the LM Guide is used in an environment where lubricant is lost, maintenance is not required if the LM guide is provided with a lubricating device QZ. The installation of options depending on the use conditions will yield a maintenance-free LM Guide.