The service life is insufficient. Can this be doubled by increasing the outer tube of the linear bushing two-fold?
Doubling the outer cylinder of the linear bushing halves the imposed load. The service life will be increased eight-fold if this is applied to the life calculation formula L= (Ca/P) 3.