Linear Ball Slide Precautions on Use
Handling
- Do not disassemble the parts. This will result in loss of functionality.
- Take care not to drop or strike the Linear Ball Slide. Doing so may cause injury or damage. Giving an impact to it could also cause damage to its function even if the product looks intact.
- When handling the product, wear protective gloves, safety shoes, etc., as necessary to ensure safety.
Precautions on Use
- Prevent foreign material, such as cutting chips or coolant, from entering the product. Failure to do so may cause damage.
- If foreign material such as cutting chips adheres to the product, replenish the lubricant after cleaning the product.
- Do not use the product at temperature of 80℃ or higher.
- The Linear Ball Slide is incorporated with a stopper mechanism that prevents the slider from coming off. If impact is given, the stopper may be damaged. Do not use this stopper as a mechanical stopper.
- Do not use undue force when fitting parts (pin, key, etc.) to the product. This may generate permanent deformation on the raceway, leading to loss of functionality.
- Insufficient rigidity or accuracy of mounting members causes the bearing load to concentrate on one point and the bearing performance will drop significantly. Accordingly, give sufficient consideration to the rigidity/accuracy of the housing and base and strength of the fixing bolts.
- Micro-strokes tend to obstruct oil film to form on the raceway in contact with the rolling element, and may lead to fretting corrosion. Take consideration using grease offering excellent fretting prevention. THK also recommends periodically executing a full stroke with the unit to ensure that the raceway and balls are coated with lubricant.
Lubrication
- Apply lubricant before using the product.
- When lubricating the product, apply grease directly on the raceway and stroke the product several times to let the grease spread inside.
- Do not mix different lubricants. Mixing greases using the same type of thickening agent may still cause adverse interaction between the two greases if they use different additives, etc.
- When using the product in locations exposed to constant vibrations or in special environments such as clean rooms, vacuum and low/high temperature, use the grease appropriate for the specification/environment.
- The consistency of grease changes according to the temperature. Take note that the slide resistance of the Linear Ball Slide also changes as the consistency of grease changes.
- After lubrication, the slide resistance of the Linear Ball Slide may increase due to the agitation resistance of grease. Be sure to perform a break-in to let the grease spread fully, before operating the machine.
- Excess grease may scatter immediately after lubrication, so wipe off scattered grease as necessary.
- The properties of grease deteriorate and its lubrication performance drops over time, so grease must be checked and added properly according to the use frequency of the machine.
- The greasing interval varies depending on the use condition and service environment. Set the final lubrication interval/amount based on the actual machine.
Installation
Linear ball slide base is installed with hex-socket-head bolt (JIS B 1176) however, models shown in Table1 to be installed with screws as shown.
| Model No. | Type | Screw model No. |
|---|---|---|
| LS 827 | Cross-recessed pan head screw |
M2 |
| LS 852 | ||
| LS 877 | ||
| LS 1050 | Low-head, small- diameter bolt * |
M3 |
- Cross-recessed pan head screw JIS B 1111
*Low-head, small-diameter bolts are not defined in the JIS standards. Select an appropriate commercially available bolt from the dimensional table.
Offset of the Cage
The cage used to hold the balls may be offset due to machine vibration, inertia, impact, etc.If the product is used under the following conditions, the cage is subject to being offset. In such cases, we recommend using model LSP or LSC.
- Vertical use
- Pneumatic cylinder drive
- Cam drive
- High speed crank drive
- Under a large moment load
- Butting the guide’s external stopper with the table
Storage
When storing the Linear Ball Slide, enclose it in a package designated by THK and store it in a room in a horizontal orientation while avoiding high temperature, low temperature and high humidity.
Disposal
Dispose of the product properly as industrial waste.