1. Home
  2. THK by Motion Type

THK by Motion Type

Linear

Every day we are surrounded by things that move in a linear fashion. At THK, our roots lie in our initial development of a Linear Motion (LM) Guide that can guide a device accurately along a straight line. This manufacturing know-how has let us keep expanding the range of linear guidance products we produce to the present day.

Caged Ball LM Guide Model SHS

Applied linear motion

Large automatic glass doors

Large automatic glass doors

Our LM guides are used for guidance of large automatic glass doors in many new intelligent office buildings. Conventional plastic resin rollers could not be used because of the increased weight of such doors and the windblast. Our LM guides solved these problems. They also make the door mechanism more compact and allow more freedom in door design.

Products

The LM Guide (Linear Motion Guide) is our main product, incorporating a part with a linear rolling motion into practical usage for the first time in the world.

The Ball Spline is a rolling guide spline bearing.

The LM Guide Actuator is a compact actuator with high rigidity and high precision that has an integrated LM Guide with a ball screw.

The Slide Pack is an inexpensive linear guide configured with the press-formed slider and roll-formed rails.

The Slide Rail is a low-priced limited-type linear guide made of steel plate precision-formed by rolling.

Oscillating

Oscillation is a movement similar to joints of the human body. Various parts are joined together and gaps that would otherwise be created by complex movements are smoothly brought together. "Joints" or "couplers" between machine parts are also well known. THK products exhibiting oscillating movements include "Link Balls," "Rod Ends" and "spherical plain bearings". In particular, our high-performance link balls have been manufactured based on our unique technologies since the formation of THK.

Link Ball Model BL

Applied oscillatory motion

Motor vehicles

Motor vehicles

THK's link balls are used in the stabilizers that are so important for the comfort and safety of automobiles. By controlling and linking the movement of the left and right suspensions, they reduce roll and stabilize the vehicle.

Products

The Link Ball is a spherical slide bearing with a ball stud that provides smooth operation with a minimal clearance.

The Rod End is a spherical slide bearing incorporating a spherical inner ring with precision and hardness equivalent to that of steel ball bearings.

The Spherical Bearing is a heavy-duty self-aligning sliding bearing

Curve

Some machines need movement not only along a straight line but also on a smooth curved line. To facilitate this, THK provides the "R Guide" and the "Straight-curved Guide" devices. These devices allow for very accurate guidance that could not have been achieved through a combination of only conventional rotary and linear motions.

Straight-curved Guide Model HMG

Applied curved motion

Large-capsule bingo game machines

Large-capsule bingo game machines

Our R guides are used in arcade bingo game machines. The large capsule is shaken and rotated to scramble the bingo's number balls. The R guides enable the machine's reliable oscillatory movements.

Crossing

By positioning two linear motions orthogonally at 90-degree angles, freer movement can be achieved. This is an expanded application of linear motion. Free movement on a plane surface is used in various fields.

Caged Ball Cross LM Guide Model SCR

Applied orthogonal motion

Seismic isolation technology for buildings

Seismic isolation technology for buildings

Quake-absorbing" technology to alleviate quake vibrations is a valuable countermeasure against earthquakes. When LM guides are combined orthogonally, they can move in a free motion on a plane surface. Combined with damping rubbers, this is the basis of THK's THK's unique quake-absorbing system. Through the know-how we have accumulated making LM guides, THK is creating new systems that can protect people's lives and property from natural disasters.

Circuit

Machine movement can be fundamentally divided into rotary and linear motions. Ball bearings are among the most famous machine parts exhibiting rotary motion, but among THK's products, the representative rotary motion device would be our "Cross-Roller Rings". These devices offer an efficiency that ball bearings do not.

Cross-Roller Ring Model RU

Applied rotary motion

Arc welding robots

Arc welding robots

Cross-roller rings are used in the rotary motion section of joints of arc welding robots on a production line of factories. Because cross-roller rings alone are rigid in the direction of each load of radial and axial moments, they can be used to develop the compact joints of robots.

Products

The Cross-Roller Ring is a roller bearing with high rotation accuracy capable of bearing loads in every direction.

The Cam Follower is a compact bearing with a high-rigidity shaft and a built-in needle bearing.

The Roller Follower is a compact bearing with a high-rigidity shaft and a built-in needle bearing.

Spiral

A spiral movement can be facilitated by rotary and linear motions. A combination of these motions allows accurate and sophisticated positioning. THK's "Ball Screw Spline" has Ball Screw nuts and Spline nuts on a single axis to allow both rotary and linear motions from one compact design.

Ball Screw / Spline Model BNS

Applied spiral motion

Scalar robots

Scalar robots

Scalar robots are used to transport and position workpieces within small areas. LM Guide systems are crucial for their high accuracy in both stroke movement and rotation on the Z axis, where high speed and low runout are essential.