Sequence Troubleshooting
Alarms
How do I use the event history?
The event history integrates the functions of logging alarm occurrences and acquiring waveforms at any given time.
The three types of functions are described below.
Types of Event History Waveforms:
When an alarm occurs: Acquire internal data for eight seconds before and two seconds after the alarm.
External event trigger: When waveform acquisition timing is indicated by the PLC, internal data is acquired for eight seconds and two seconds after that timing.
Acquire present waveform data: This function is run from T-ACT. When selected during trial run sequence, or when the button is clicked on the event history screen, the waveforms for 10 seconds from that point are acquired.
In each case, waveforms that have been successfully acquired are marked with a ★ symbol and can be read back into the application by selecting the history. Up to 32 history data items can be retained.
* This waveform data is retained in the controller, but because it is buffered in volatile memory, it cannot be read back when the controller is turned off and on again.
I want to know how to check alarm codes. I want to learn the details of an alarm.
Alarm codes can be found on the event history screen of the T-ACT PC application.
The (0x●●) portion of the displayed list is the detailed alarm code.
For the meaning of each code, you can check the event code list by clicking on the "?" mark.
For details, please refer to "6-6. Event history function" and "8-1. Event list" in the instruction manual.
Stopping
What is the operation when a stop is entered?
The following operations are performed in each module.
Z axis and θ axis: Stops according to the acceleration and deceleration coefficient set in the sequence.
Air drive: Maintains the same status as when stopped.
Sensor: Cancels the target value judge setting.
Status: When the sequence is stopped by a stop input, a sequence stop signal is output. At this time, no timeout signal is output.
Emergency Stop
Tell me about the emergency stop.
Emergency stop is performed by turning off the 24 V power supplied to the controller.
Operation of Each Axis:
Z axis: Servo turns off immediately and the Z axis brakes.
If the operation is being performed at high speed in the downward direction, there is a possibility that inertia may cause it to drop slightly.
Θ axis: Servo turns off immediately. Θ axis has no brake, so it rotates through inertia, loses momentum, and then stops.
Air drive: Both the vacuum valve and the release valve turn off.
During workpiece suction, negative pressure gradually decreases through the gaps in the vacuum structure.
Please contact us for further information regarding the emergency stop.
Home Return
Is homing required when the power turns off?
Homing is required.
Because an incremental encoder is used, the home position is forgotten when the power is turned off.
Also note that homing is generally required when an alarm occurs.
(Alarms for which the home status in the event list in section 8-1-1 of the instruction manual is reset require homing after alarm occurrence.)
Sequence
A timeout has occurred. I would like to investigate the cause.
Confirm the waveform on the monitor and event history screens.
When the timeout occurred, which module was the last module in operation? If that step operates and a timeout occurs, it is very like that it is stopping at the following step.
If you send us the waveform data, we will be able to assist you in your investigation.
What is the method of confirming workpiece suction?
As for the PPR's sequence, it is possible, for example, to determine whether suction has occurred with a pressure sensor.
The various sensor values are transmitted to the host PC/PLC via cyclic communications so that the PC/PLC can also utilize these sensors values.
The timing determined by the pressure sensor can be communicated as a step completion signal.
How do I shorten the cycle time?
Here are some example ideas of how to shorten the operation of the picking template.
(1) Speed up the Z axis positioning operation.
(2) Adjust the starting position of the contact stop and shorten the stroke of the contact stop.
Or, increase the speed of the contact stop (make sure that the impact force on the workpiece is in an acceptable range at this time).
(3) Lower the judgment threshold value setting for the pressure sensor.
We can check your actual operations and provide you with improvement proposals if you provide us with the waveform data and information on the current program.
Tell me about judging the failure of suction/release.
For example, for the following judgments:
- Picking operation failure is determined by whether suction is completed within a certain period of time after the solenoid valve is turned on.
- Placing operation failure is determined by whether pressure is restored after vacuum breakage.
Both can use the timeout judgment in the pressure module.
When the pressure module is operated after the operation of the air drive, it judges whether the pressure reaches the set value.
At this time, if the set time for timeout elapses, the judgment will be a failure. When the timeout operation setting is set to stop, sequence stop will be output to the PLC, so when this signal is output, it can be assumed that suction or release has failed.
I want to judge a part as an error (judged by height at time of contact).
We propose two methods.
Method 1: Perform height judgment at contact stop in the PPR's sequence program
Method 2: Set everything until contact stop as a single sequence, and judge height with the PLC when stopped.
You can also consult with us on how to program other operations that you wish to achieve.
The sequence stops midway. (There is no change in the pressure sensor. / The solenoid valve is working.)
Upon confirmation of the monitor waveform, no change was observed in the pressure sensor.
However, the solenoid valve is working.
Possible causes in this situation are as follows:
・The vacuum pump is not working normally.
・It is not properly piped for suction air.
・The solenoid valve is malfunctioning.
We can confirm and analyze the actual operation if you provide us with waveform data and information on the program at the time of occurrence.
The sequence stopped partway through. (It failed to make contact.)
Upon confirmation of the monitor waveform, the STEP2 contact stop on the Z axis was the last operation. There is also no change in the value of the force sensor when the machine stops, and the Z axis has reached the contact failure position.
The reason for this may be that the Z axis contact stop operation did not contact the workpiece and instead failed to make contact. The following situations are possibilities, so please confirm the status.
・There is no workpiece.
・The target position of the sequence was just short of reaching the workpiece.
・Because the home position was changed in the user home settings, the workpiece was not reached due to a change in the arrival position.
We can confirm and analyze the actual operation if you provide us with waveform data and information on the program at the time of occurrence.
Click here for other questions
Basic Specifications