- How can I reduce the sliding resistance of an LM Guide?
- The following measures can be taken to reduce sliding resistance.
Seals
- Consider using an LM block without seals. In addition, end seals (LL seals) with low sealing resistance are available for some models.
Clearance
- Since sliding resistance increases with greater preload, to reduce sliding resistance, consider a clearance with a smaller preload.
Grease
- Consider selecting a grease with low viscous resistance or using oil lubrication.
We also offer the Model EPF, which has a finite stroke, low sliding resistance, and does not circulate balls.
For the table of supported options by model, click here