Copy item link
Add item to favorites
What is the orientation of the grease nipple on the LM block?
The LM block is installed so that the lubrication port faces away from the reference surface and toward the side with the THK mark.
Please specify at the time of purchase if you have a preferred orientation for the lubrication port.

    For LM Guide reference surfaces, click here.