- What does the "-II" symbol for the number of axes used on the same plane mean in the LM Guide model number?
- This symbol is added to the model number when two parallel axes are used on the same plane.
Smooth movement is achieved by maintaining precision in the relative height and width between the two axes.
When purchasing, add the "symbol for the number of axes used on the same plane" to the model number and order the number of sets to be used in parallel.
(For example, two sets of "-II" are required for two parallel axes.)
For accuracy standards, click here.