Linear Ball Slide
With Rack Model LSP
This model is based on that of LS type but has an added feature of a rack and pinion mechanism on the cage which prevents cage creep.
Without Rack Model LS
This is a highly corrosion resistant slide unit which includes stianless steel balls with an extremely small friction coefficient resulting from the needle roller raceways.
With Rack Model LSC
This style includes an integral air cylinder in it's base to provide drive. Feeding air into the two ports on the side face of the base allows the slide to perform reciprocating motion.