Skip to Contents


TRANG CHỦ > Now Accepting Orders for the Utility Slide Advanced Wheel Guide

November 19, 2024 

Now Accepting Orders for the Utility Slide Advanced Wheel Guide: A Smooth Slide Mechanism That Uses Wheels for the Rolling Elements

 THK has begun accepting orders for the Advanced Wheel Guide utility slide, which uses wheels for its rolling components, for the railway and logistics industries.

Advanced Wheel Guide

 The Advanced Wheel Guide is a utility slide composed of an outer member and a carriage with mounted wheels.

 Possessing the aligning function that THK has developed with the LM Guide, it can absorb error present in rough installations and provide long-term, smooth, and stable guiding motion. Additionally, thanks to superior contamination prevention provided by a proprietary scraper, it can even be used in adverse environments.

 While conventional slide rails have seen wide application as sliding elements for medical and office devices, the Advanced Wheel Guide is targeted at the railway and logistics industries. It is projected to see demand for use in rail car doors, automated warehouse racks at distribution centers, and the opening and closing elements of machine tool doors.

 THK will continue to use the technology and expertise it has cultivated as a top machine component manufacturer to provide optimal solutions to the challenges faced by customers in a wide range of fields, including those in the railway and logistics industries.

catalogdownload

For availability please contact your local THK dealer.

Please create a free account to our Technical Support Site to download catalogs.
>Create a free account

Advanced Wheel Guide Example Applications

Advanced Wheel Guide Example Applications

Features

Smooth Sliding Mechanism

 The alignment function created by the circular arc structure, in which the outer member and wheels make contact at two points, enables smooth sliding motion even when installed onto surfaces with low accuracy.

Smooth Sliding Mechanism

Superior Contamination Protection

 The proprietary scrapers on the ends of the carriage are capable of maintaining contact with the raceway surface for a long time, which grants superior contamination protection compared to slide rails.

Environmentally Conscious Lubrication System

 The proprietary grease tank structure is an environmentally conscious lubrication system that reduces the application of excess grease and avoids contaminating the surrounding area by applying an appropriate amount of grease to the raceway.

 

catalogdownload

For availability please contact your local THK dealer.

Please create a free account to our Technical Support Site to download catalogs.
>Create a free account

  THK Vietnam Hanoi Sales Office 
Phòng số 101, Tầng 17, Tòa nhà VIT, số 519 Kim Mã, phường Giảng Võ, thành phố Hà Nội,Việt Nam
Số điện thoại: +84-222-373-4974 (Tiếng Việt, Tiếng Anh, Tiếng Nhật đều sẵn sàng)
* Các hỏi hàng bằng tiếng Trung Quốc có thể được hỗ trợ bởi ZALO Official
Số điện thoại Người Nhật: +84-904-481-199
Email : sales-support@tmv.thk.com
HQ: THK Manufacturing of Vietnam CO., LTD. Bac Ninh branch

zalo